Dear users, due to planned maintenance work you might not be able to see product search results, beginning from today (24/09/2024) 10:00 PM CET. We aim to have the full functionality restored by 2:00 AM CET.
Innovative charging technology from a single source
Equip your charging points with CHARX from Phoenix Contact: As a component manufacturer, we supply all the equipment for your charging infrastructure – whether an AC home charger, DC fast charging station, or HPC charging park, whether in PCB, DIN rail, or 19" rack mounting. Our broad portfolio – from CCS charging cables through to load management – forms the basis for a high-performance charging network for electric cars.
Pure e-mobility is a key factor on the path to the All Electric Society. A convenient and carbon-neutral charging process not only requires a fast charging network for electric vehicles, but also coupling with other sectors. With our high-performance and intelligent CHARX products, we will ready you for the e-mobility of the future – sustainable, networked, and practical.
Charge
Our product recommendations for safe, fast, and convenient charging of electric vehicles in all everyday situations:
NACS is coming – and we’re prepared
AC and DC charging cables for the most demanding requirements
The North American Charging Standard (NACS) is gaining momentum and will replace the type 1 CCS charging standard in the long term. NACS will therefore play a central role in the electrification of the transport sector and the ramp-up of charging infrastructure in North America.
As a specialist in e-mobility charging technology, we of course want to satisfy the changing requirements of our customers and therefore offer SAE-compliant and UL-certified NACS charging cables that meet the particularly high demands – both for AC charging and for High Power Charging.
Reliable connection technology for your PCB-based home chargers
Optimally integrate power and data
Our connection technology for PCB-based home chargers and charging stations enables you to rapidly connect grid feed-in, charging cables, and data cables so you can easily set up an installation on site. Short installation times, permanently secure connections, and low maintenance costs increase the availability and cost-effectiveness of your charging infrastructure.
Discover our extensive charging technology portfolio for electric vehicles and charging infrastructure on over 160 pages. You can also find out everything you need to know about our company and learn the basic principles of charging technology.
Your advantages
Why Phoenix Contact is the right choice
We will assist you in developing your charging infrastructure project: with a broad portfolio, professional product selection and engineering consultation, practical application examples, and expert know-how. If needed, we will also develop customer-specific solutions or even new technologies. We are there for you worldwide, also in your vicinity.
The uniform, modular product design and tool-free connection technologies such as Push-in and Push-X allow you to install and wire the components in the charging station in a quick, convenient, and space-saving way. A special panel feed-through ensures easy installation of the HPC charging cable. With maintenance-friendly and replaceable product components you are going to save both time and money during service works.
As the pioneers of fast charging technology we develop future-oriented technologies like High Power Charging (HPC) and, with that, enable short charging times that are suitable for everyday use. Reliable charging connection systems and charging controllers as well as high-performance power supplies, protective devices, and cybersecurity products guarantee safe, economic 24/7 operation of your charging infrastructure.
Network your charging points with communicative products, open standard protocols, and established interfaces such as Modbus/TCP, REST, MQTT, or OCPP (Open Charge Point Protocol). Implement a convenient controlling and transparent monitoring of your charging park inclusive of load management, as well as a seamless connection to building management and backend systems. Charging connector status and usage data allow preventive planning of maintenance when it comes to wear and tear.
Depending on the number, charging power, and scope of functions of your charging points, you can choose the appropriate product combination from our scalable portfolio. With modular charging controllers and power electronics as well as graded software licenses and over-the-air updates, you are well prepared for future developments and extensions of your charging park.
Our current commercial spot
From a home charger to a fast charging park
Our scalable portfolio allows you to realize any charging solution
Companies
Charging opportunities for employees, guests, and the vehicle fleet require load management and are often integrated into the building and energy management system. The typical charging powers here are 22 kW AC and 150 kW DC. Operation is usually via a central terminal with user authorization. The billing of charging processes and remote maintenance of the charging stations can be implemented as an option.
Towns and municipalities
A comprehensive charging network in urban areas serves to reduce emissions and thus improve the quality of life. The typical charging powers here are 22 kW AC and 150 kW DC. User authorization, billing of charging processes, and remote maintenance of the charging points are required. A touch panel or buttons can be integrated into the charging stations for operation as an option.
Hotels, shops, and restaurants
Charging opportunities provide added value for guests and promote customer loyalty, especially if charging is offered free of charge. Due to the longer duration of their stay, charging is usually performed with 11 or 22 kW AC. For customers who are in a hurry, DC charging with, e.g., 50 kW can be offered as an option. A load management system is required in the case of multiple charging points. Various billing and remote maintenance options as well as integration into the building management system round out the charging solution.
Rental apartments
Charging stations for tenants usually offer 11 kW AC. So as not to overload the building connection, an energy management system is used in the case of multiple stations. Direct billing of individual charging processes is not necessary if the electricity consumed is read on separate energy meters and paid via the annual service charge settlement. To prevent electricity theft, however, it makes sense to restrict access or authorize users.
Private residential buildings
Home chargers for garages and carports usually charge with 11 kW AC. However, there is also a trend towards DC home chargers with 22 kW, which can use the direct current of a photovoltaic system with only minimal conversion losses. As an option, the home charger can be integrated into a smart home system to which the photovoltaic system and energy storage system are also connected. This enables intelligent, PV-optimized charging.
Parking lots and parking garages
There are several charging points in a small space and an operator terminal for user authorization. Charging is typically performed with 11 to 22 kW AC and optionally with DC. Functions such as dynamic load management, precise billing of charging processes, and the option of remote maintenance in the event of faults are essential for smooth operation. Integration into an energy management system also makes sense if there are other loads in the building or there is a photovoltaic system on the roof.
Vehicle fleets
When it comes to the fast charging of passenger, transport, and utility vehicles, the focus is on cost-effectiveness and thus the capacity utilization and tight scheduling of the vehicles. This requires short charging times and high charging powers of typically 22 kW AC and 400 kW DC. User authorization, load management, remote maintenance, and building integration are required for safe, reliable, and smart operation.
Fast charging parks, service stations, and rest areas
These public charging stations are usually located on highways and main transport hubs and offer High Power Charging (HPC) with up to 400 kW DC to enable fast onward travel after a few minutes of charging. Each charging station has its own screen for convenient operation. Authorization and billing are performed via an app, charge card, or credit card. Dynamic load management and remote diagnostics are essential for safe and reliable 24/7 operation.
Successfully completed customer projects
Find out how we have implemented exciting projects together with customers and partners
Charging park with intelligent load management: German company GP Joule specializes in renewable energies and has equipped its on-site charging park with a load and energy management system. The objective: to charge the company’s fleet of 28 electric cars, making optimum use of self-generated biogas and solar power. Everything is controlled via a central control cabinet equipped with AC charging controllers, energy meters, and software from Phoenix Contact.
DC home chargers for bidirectional charging: Swiss company Evtec relies on bidirectional charging for its new charging stations. This allows the electric vehicle to be charged via self-generated solar power and for power to be fed back into the building at night. Our CCS charging cables CHARX connect compact, which were developed specifically for DC charging in the home environment with lower charging powers of up to 80 kW, are used here.
Sustainable designer charging stations made of stainless steel: German family-owned company hesotec electrify not only focuses on quality and design, but also sustainability. With its timeless designer charging stations made of stainless steel, the company offers recyclable AC charging solutions for sophisticated requirements – from both a visual and technical point of view. Our multi-award-winning designer charging cables CHARX connect comfort and our charging sockets CHARX connect modular are the perfect match.
Southern Europe’s largest HPC charging park: Ingeteam is a company empowering e-mobility – and not just in Spain, where the company has been working toward the electrification of a sustainable future for the past twelve years. At a transport hub in southern Spain, Ingeteam’s fast charging stations with a nominal power of 4 MW enable a vehicle to be charged in approximately five minutes. The company uses the HPC charging cables CHARX connect professional from Phoenix Contact for this.
Research project enables ultra-fast charging: Together with BMW, Porsche, Siemens, and Allego, we have developed, created, and launched the world’s first HPC charging station with a charging power of 450 kW as a part of the FastCharge research project. To promote widespread acceptance of e-mobility, the project demonstrated that ultra-fast charging works in practice. We supplied our liquid-cooled HPC charging cables CHARX connect professional, as well as the control technology for this project.
The first on-demand mobile fast charging service: with a mission to provide green energy for all, everywhere, Italian company E-GAP is present in several major European cities, supplying electric car owners with the amount of energy requested via an app. The modular charging system in the E-GAP vans contains everything for AC and DC charging of electric vehicles with up to 80 kW and is equipped with charging technology, energy meters, and connection technology from Phoenix Contact.
Charging stations with a remarkable CO₂ balance: Velocity, a German provider of rental mobility systems, has developed a charging solution for its electric cars and bikes together with Pion Technology. The concrete material used for the charging station housings filters particulate matter out of the surrounding air and therefore achieves a remarkable ecological balance. Along with our AC charging technology and power supplies, Pion Technology also uses our communication technology for cloud-based billing.
With CHARX, our charging solutions can be used flexibly in different environments in charging parks. We can use it to offer our growing customer base a complete solution, from analysis, planning, and implementation, all the way to operation.
High Power Charging reinvented
Megawatt charging with CCS
Our CCS charging cables featuring the latest HPC technology take ultra-fast charging of electric cars and utility vehicles to a new level. A newly developed cooling concept enables CCS charging with up to 1,000 kW for the first time. Learn more about how this technology works.
I will be happy to advise you on your charging infrastructure project.
Phoenix Contact E-Mobility
Your powerful and reliable partner
Phoenix Contact E-Mobility has been the specialist for e-mobility charging technology within the Phoenix Contact Group since its founding in 2013. With more than 800 employees worldwide and 25 production lines over an area of 33,200 m², we offer more than 500 products for the development of a networked charging infrastructure and for the electrification of vehicles. With IATF certification, the company meets the high requirements of the automotive industry.