Our products and solutions are paving the way toward a climate-neutral and sustainable future.
You will find information on new products and the latest news from Phoenix Contact here.
Phoenix Contact is expanding its Ethernet-APL portfolio to include two managed switch versions with twelve ports for process automation.
With the new Sunclix crimp contacts for conductor cross-sections from 6 to 10 mm², Phoenix Contact is expanding its portfolio for powerful DC connections.
Phoenix Contact has expanded its portfolio of KNX power supply units to include a new 1,280 mA version that complements the proven 640 mA model. The KNX bus power supplies offer system integrators and building automation specialists robust power supply solutions.
With the VAL-SPP-T1-1500DC-PV-2+V-UT-R lightning current arrester, Phoenix Contact has added a type 1 lightning current arrester for photovoltaic systems with 1,500 V DC to its Safe Protection Plus product family.
Phoenix Contact will be exhibiting again at this year’s edition of Europe’s largest energy industry platform, “The smarter E Europe”. The company will be showcasing solutions for a sustainable, cross-sector power supply in Munich, Germany, from June 23 to June 25, 2026, in line with the trade fair motto “Accelerating Integrated Energy Solutions”.
Phoenix Contact is extending the range of functions of its CHARX control modular AC charging controllers: With automated authentication in accordance with ISO 15118-2 (plug-and-charge) and guided initial configuration via app, the controllers support additional features for the standard-compliant operation of AC charging infrastructure.