To further sharpen and holistically align its global sales activities with customers and markets, Phoenix Contact is expanding its Group Executive Board with the newly established role of Chief Sales Officer (CSO). Effective May 15, 2026, Stephan Volgmann will assume this position within the Group Executive Board.
News Keep up-to-date with the latest news about our products and technologies, our company, our strategic business development, and our sustainable commitment. You can download press information and image material conveniently in the download area.
- Filters:
-
Topic area
-
Topic
-
Product category
Phoenix Contact strengthens its global sales organization: Position of Chief Sales Officer established within the Group Executive Board
Push-X product program continues to grow
Phoenix Contact is extending its XT product range to include terminal blocks with a nominal cross-section of 4 mm². This enables consistent, tool-free wiring for conductor cross-sections from 0.34 to 25 mm².
Current monitoring made easy
With the new CMU DC current measuring unit, Phoenix Contact offers a clearly understandable and compact solution for current monitoring. Existing systems can be extended easily to include practical energy and utilization monitoring due to their bridgeability.
Innovative plug-in test systems for the energy transition
With Fame LPIT, Phoenix Contact is presenting a new generation of plug-in test systems for low-power sensors in medium and high-voltage switchgear. The solution enables the fast, safe, and convenient testing of modern protective systems.
The new generation of safety relays – PSRcompact: compact, efficient, and safe up to SIL 3 and PL e
Phoenix Contact is further extending its portfolio of safety relay modules with the new PSRcompact safety relay. The product family provides up to five enabling current paths in one space-saving housing. This makes the devices ideal for use in modern machine building and systems manufacturing concepts.
Ergonomics and productivity combined in a new mounting bench
More than ever before, efficiency is becoming a decisive factor in control cabinet building. The shortage of skilled workers and increasing demands on ergonomics are forcing companies to rethink their production concepts. They are increasingly looking for flexible solutions to make their mounting and wiring processes more efficient and ergonomic at the same time.
Sustainable marking material for all control cabinet components
In response to the growing demand for sustainable solutions, Phoenix Contact is launching a comprehensive portfolio of sustainable marking materials for industrial identification.
NE-95-certified signal conditioners and measuring transducers for demanding process industry applications
Phoenix Contact is now providing complete, up-to-date NE-95 test reports for selected devices from the Mini Analog Pro and Macx Analog families of signal conditioners. The tests were carried out in accordance with the NAMUR recommendation NE 95 “Test methods for automation technology devices”. They confirm the high robustness, accuracy, and interoperability of the signal isolators in industrial use. The reports serve as a neutral basis for decision-making and support users with inquiries, approvals, and tenders. They often replace in-house function or integration tests.
Phoenix Contact sells Perle Systems Ltd. to Hitron Technologies Inc.
Phoenix Contact has entered into an agreement to sell Perle Systems Ltd. and its subsidiaries to Hitron Technologies Inc. The transaction represents an important step in Phoenix Contact’s strategic focus on its core businesses.
First phase of construction for Phoenix Contact’s new Mexican production facility in Querétaro officially inaugurated
To strategically expand Phoenix Contact’s global production network, improve supply chains, and be even closer to its target markets, the company has expanded its production network on the American continent. Production has now begun at the site in Querétaro, Mexico, as part of the first phase of construction.
Phoenix Contact and Symcon enter into a technology partnership for open building automation
To further advance open, interoperable building automation, Phoenix Contact and Symcon have entered into a technology partnership. The goal of this collaboration is to provide planners, system integrators, and electrically skilled persons with an efficient path from hardware through software to ongoing operation.
The Emalytics building management system is the key to the digital transformation in facility management
The long-term goal is to make all building data available centrally and consistently throughout its entire lifecycle. This requires a fully digitalized engineering process in which information is entered only once, stored in a structured manner, and processed across systems.
Surge protection for the busbar with integrated voltage pick-off
The new FLT-SEC-ZP2-…-SV combined lightning current and surge arrester from Phoenix Contact sets new standards in the protection of meter panels: The low overall width of the surge protection leaves plenty of space for the other components mounted on the busbar.
New safety relay module for potentially explosive areas
With the new PSR-MC35-EXI safety relay, Phoenix Contact is further expanding its safety portfolio. The product enables safe operation in demanding industrial environments. It was specifically developed for use in zone 2 potentially explosive areas. The device also has IECEx and ATEX approval and therefore meets international safety requirements.
Hybrid connector for energy storage
Designed for customer-specific assembly, the hybrid connector for electrical energy storage systems from Phoenix Contact provides a reliable and safe connection for power, signal, and data contacts. The new all-in-one solution offers cost-optimized and time-efficient installation that is specifically tailored to the customer’s needs.
Sunclix DC connectors approved for 2,000 V DC in accordance with new TÜV test specification
The Sunclix DC connectors from Phoenix Contact are now approved for a system voltage of up to 2,000 V DC in accordance with the TÜV Rheinland 2 PfG 2925/01.23 test specification.
M12 power device connectors with push-pull fast locking
The new M12 push-pull power device connectors from Phoenix Contact extend the existing portfolio with a compact solution for reliable power transmission.
Cutting tool for busbars and standard DIN rails
Profile and rail cutters from Phoenix Contact enable standard DIN rails and cable ducts to be cut to length quickly, precisely, and burr-free. Due to the optimal lever ratio, cutting requires minimal effort and is easy on the joints, while the chip-free cut ensures a clean workspace and eliminates the need for rework.
Best of Industry Award for PSRuni multifunctional safety relay
Major recognition for innovative safety of machinery: The PSRuni multifunctional safety relay was awarded the Best of Industry Award 2025 in the “Modular Machine Concept” category. The solution impressed users and industry experts alike and prevailed over strong competitors in Vogel-Verlag’s public online vote.
Phoenix Contact E-Mobility undergoes strategic realignment and exits the automobile OEM business: Asset deal with the TE Connectivity Group marks an important milestone in the company’s transformation.
Phoenix Contact E-Mobility has reached an important milestone in its strategic transformation with its planned exit from the passenger car business (OEM automotive). As part of an asset deal, the TE Connectivity Group is acquiring significant assets and activities in connection with Phoenix Contact E-Mobility’s business with passenger car manufacturers.
Phoenix Contact at Hannover Messe: It’s all about comprehensive, networked energy systems
At this year’s trade fair, Phoenix Contact is focusing on four topics: Power Reliability, safe automation, efficient control cabinet building, and integrated connection technology. The family-run company will be exhibiting its products and solutions for the first time in Automation Hall 27, Booth G26, in line with the new Hannover Messe exhibition concept.
New access point with Wi-Fi 6 for industrial automation
Phoenix Contact is extending its industrial wireless portfolio with new access points from the WLAN 2300 series, which support Wi-Fi 6 functions in accordance with IEEE 802.11ax. The devices can be used to create efficient and powerful WLAN networks with up to 100 devices per virtual access point interface.
New speed starter for motors up to 7.5 kW extends the scope of application
The new speed starter in the Contactron series from Phoenix Contact is suitable for motors up to 7.5 kW and offers flexible speed control as well as high safety standards (SIL 3/PLe). Installation is quick and easy thanks to intuitive operation and simple wiring.
Plug-and-play upgrade without rewiring: I/O signals can be migrated quickly and safely with Varioface
With the new Varioface Migration Solution, Phoenix Contact presents a completely pluggable solution for efficiently upgrading to the ET 200SP HA controller. Integration is seamless and does not require any modifications to the control cabinet or changes to the existing field wiring.
Smart Ethernet Box with improved outdoor housing and lock adapter
The Smart Ethernet Box from Phoenix Contact is a powerful outdoor PoE switch for demanding environments. New features include optimized housing functions and a lock adapter, which simplify installation, servicing, and access protection.
New PP-RJ-... patch panel versions with IECEx and other approvals
Four PP-RJ-…-E versions have been added to the proven PP-RJ-… series of patch panel devices from Phoenix Contact. The new models are functionally identical to the previous versions, but offer clear added value: They have all the relevant approvals such as UL, UL HazLoc, DNV-GL, ATEX, and now also IECEx.
Catan building automation portfolio receives Cradle to Cradle certification
The Catan building automation portfolio from Phoenix Contact has become the first building control system to be awarded the Cradle to Cradle Certified® Bronze sustainability certificate.
A world first in High Power Charging: Phoenix Contact integrates the charging controller directly into a CCS charging inlet for the first time
The CHARX connect advanced CCS charging inlet from Phoenix Contact sets a new standard for charging heavy electric vehicles – with integrated controller, detachable HV cables, reduced integration effort, and a high degree of future-proofing.
New HPC charging cables for North America: Phoenix Contact expands portfolio with NACS and CCS type 1 for fast charging up to 500 kW
Phoenix Contact presents an expanded DC fast charging portfolio for the North American market, offering new NACS and CCS type 1 charging cables, standard-compliant safety, a robust ergonomic design, and a clear vision for the future.
SPS 2025: The world’s first AI-generated control cabinet – produced by Phoenix Contact
The AI-generated demonstration cabinet, which was shown for the first time at SPS 2025, was created as part of a joint project between WSCAD, ABB, Phoenix Contact, and häwa.
Protective covers for CCS charging inlets – optimum protection with smart features
With maximum protection and simple operation, they set new standards for the everyday usability of electric utility vehicles: the new protective covers for CHARX connect universal CCS charging inlets from Phoenix Contact.
Ergonomic mounting device for terminal strip production
The ergonomic BS-DIN Rail Fixture mounting device from Phoenix Contact enables terminal strips to be produced conveniently and reliably. Screw-in clamping blocks reliably hold the DIN rail in place, leaving both hands free for assembly.
M8 and M12 device connectors for automated production processes
Phoenix Contact is extending its range of device connectors for the transmission of data, signals, and power. The new M8 and M12 versions are suitable for direct integration into SMT soldering processes.
Battery holder for OCS and POS housings
The new OCS Bat Hold battery holder from Phoenix Contact is specially designed for the OCS and POS series electronics housings.
Managed switches from Phoenix Contact receive IEC 62443-4-2 certification
The managed switches of the FL Switch 2000 product family from Phoenix Contact have been certified by TÜV Rheinland in accordance with IEC 62443-4-2. This confirms that the devices meet the high safety requirements demanded for automation systems.
Phoenix Contact aligns its structures even more internationally and brings its value creation closer to the sales markets
Ulrich Leidecker spoke about the ongoing economic tensions in Germany at this year's Phoenix Contact press conference held at the SPS automation trade fair in Nuremberg, Germany, from November 25 to 27.
The future of process heating: Phoenix Contact is setting a new standard for safe automation in industrial process heating
The PLCnext Technology ecosystem from Phoenix Contact now satisfies globally applicable standards such as DIN EN ISO 13577-2/4 and NFPA 85, 86, 87 for industrial process heating.
Installation contactors and installation relays for buildings
Installation contactors and installation relays are characterized by their high reliability and efficiency. They are particularly suitable for use in electrical systems in the field of building automation.
Phoenix Contact extends its device protection portfolio: Thermal-magnetic protection with a width of just 8 mm
With PTCB TM, Phoenix Contact is launching a new generation of thermal-magnetic circuit-breakers onto the market. With a width of just 8 mm, alignable current monitoring, and the capability of direct bridging to the CLIPLINE complete system, the product family ensures high efficiency and transparency in the control cabinet and is suitable for demanding industrial applications.
Simple signal cabling with M12 push-pull connectors
Phoenix Contact is extending its product portfolio to include A-coded, eight-position, pre-assembled signal cables with M12 push-pull connectors. These enable simple and fast signal cabling.
Preassembled M12 push-pull connectors for Ethernet applications
Phoenix Contact is presenting the new M12 push-pull network cables, which enable simple and reliable high-speed data transmission for Ethernet applications.
Touch-protected PCB connectors with screw connection
The PC 16 HC series with extended touch protection from Phoenix Contact now also features classic screw connection technology for worldwide use.
Maintenance-free DC UPS with integrated power supply and capacitive energy storage unit
Increasing digitalization with dynamic processes and rising electricity consumption are pushing supply networks to their limits.
M23 hybrid device connectors for wave soldering processes
The new M23 hybrid device connectors for wave soldering processes come as a space-saving 3-in-1 solution. They enable the reliable transmission of signals, data, and power in just one single connector.
Virtual PLCnext Control: A software-based controller for the industrial future
With Virtual PLCnext Control, Phoenix Contact is launching a software-based controller solution that enables flexible automation functions in virtualized IT environments.
New outdoor web panels of the WP 6000 product family
The new web panel from Phoenix Contact’s WP 6000 product family has been specially designed for use in extreme outdoor conditions.
New EP4200 and EP5200 Layer 2 raptor switches
The EP4200 and EP5200 series raptor switches from Phoenix Contact feature advanced Layer 2 functions with high performance and availability. They have been specially designed for demanding applications in critical infrastructures and in the energy sector.
Cellulink outdoor cellular routers: cybersecurity now also for potentially explosive areas
The Cellulink outdoor cellular router product range from Phoenix Contact is being extended: New versions are now also available that have been specially developed for use in Zone 2 potentially explosive areas. The devices have IECEx and ATEX approval and therefore enable secure operation in demanding industrial environments.
Reinventing automation with relays: The network-capable PLC-Interface Ethernet Gateway remote relay system with multi-protocol connection to the controller
The modular PLC-Interface Ethernet Gateway remote relay system from Phoenix Contact with flexible channel assignment optimizes simple applications with up to 56 I/O channels. The compatibility with common controller software makes a high level of flexibility and intuitive network integration possible.
Foresight instead of hindsight: Phoenix Contact brings machine learning forecasts into energy management
Phoenix Contact is extending its Energy Management Service to include a powerful forecasting function. With the help of machine learning, companies can estimate their future energy consumption, create transparency, and identify potential excess consumption at an early stage – the next step toward predictive energy management in accordance with ISO 50001.
M17 PRO hybrid connectors in accordance with the IEC standard
The new M17 PRO hybrid connector in accordance with the IEC 61076-2-117 standard from Phoenix Contact is the new benchmark in terms of compatibility and flexibility.
Click-in module carrier frames for heavy-duty connectors
The new Heavycon series click-in module carrier frame from Phoenix Contact simplifies the assembly and installation of heavy-duty connectors significantly. The tool-free click-in latching system enables the inserts to be mounted quickly and reliably – without any screws.
Terminal blocks with Push-X technology for wiring from 0.34 mm²
The Push-X product range is growing: With the new XT 1,5 terminal blocks, Phoenix Contact is extending the series to include versions for conductor cross-sections from 0.34 to 2.5 mm².
Heavycon power contact insert modules for high-current applications
The new Heavycon power contact insert modules from Phoenix Contact have been specially developed for high-current applications up to 300 A. Combining them with other modules for signal, data, and power transmission in one housing creates a highly compact interface.
Software update for AC charging controllers: CHARX control modular now with comprehensive cybersecurity functions
The CHARX control modular AC charging controller from Phoenix Contact is the centerpiece of intelligent and future-proof charging infrastructure. With the new software release 1.8, it not only meets the current requirements of the RED Directive, but is also well prepared for the upcoming Cyber Resilience Act (CRA).
Data interfaces for control cabinets and devices
The new Data Service Interfaces (DSIs) from Phoenix Contact are a convenient solution for service work on control cabinets and devices. With various interfaces including RJ45 and USB, the space-saving service interfaces enable the quick and easy connection of additional electrical devices.
New mount for photovoltaics panels – quick to install, flexible in use
The new POS Panelfix mounts from Phoenix Contact enables PV panels in the 20 to 200 Wp range to be mounted quickly and easily, regardless of the manufacturer.
New surge protection for North American power supply systems
With Valvetrab US-SPP, Phoenix Contact is extending the Safe Protection Plus product family to include UL-listed surge protection devices for the North American market. The devices are suitable for all common supply system configurations in accordance with the NEMA standard.
New online configurator for heavy-duty connectors
The Heavycon configurator is an online tool for the simple, fast and secure configuration of heavy-duty connectors. Even experts sometimes have problems choosing the right solution simply because of the large number of possible combinations. The configurator supports users in the selection, validation, and visualization of connectors, and saves valuable time in the project business.
Power supply for panel mounting now also with Push-in connection
The Trio Power power supplies for panel mounting with an output of up to 2.5 kW now feature Push-in connection. The devices with an output voltage of 24 or 48 V DC are characterized by their high power density and efficiency in a compact design.
Modular AC charging sockets with a reduced installation depth – for flexible and space-saving mounting
The CHARX connect modular type 2 charging sockets from Phoenix Contact are now available with a reduced installation depth: With the third generation, the company is launching an optimized solution for flexible and space-saving integration into charging infrastructure solutions.
New configurable signal towers with IO-Link interface
Phoenix Contact is extending its portfolio of signaling devices with three new configurable signal towers of the PSD-SC series. The models feature up to 15 RGB segments, various operating modes, and can be configured conveniently via the IO-Link interface.
Compact LED signal lights for direct machine integration
The new PSD-SL LED signal light series by Phoenix Contact is a compact solution for application-oriented signaling directly on machine functions. The lights are versatile, robustly built and suitable for both indoor and outdoor use.
Unshielded board-to-board connectors with a 0.8 mm pitch
Phoenix Contact is presenting the new unshielded board-to-board connectors of the FP 0.8 SL series for data rates of up to 52 Gbps. The connectors enable increased flexibility in PCB design thanks to their compatibility with the PCB footprints of the shielded FP-0.8 versions. The designer can switch between shielded and unshielded versions without having to adapt the PCB layout.
Grundfos recognizes Phoenix Contact with the Sustainability Direct Award
Phoenix Contact has received the Sustainability Direct Award from Grundfos. This award recognizes the Blomberg-based company’s commitment to sustainability as an integral part of its business operations and innovation activities.
Battery modules with lithium iron phosphate technology
With the new lithium battery modules with IQ Technology, Phoenix Contact is expanding its portfolio with powerful energy storage solutions with a capacity of 284 Wh.
Function extensions for AC charging controllers: New calibration law concept simplifies certification via software update
The CHARX control modular AC charging controllers from Phoenix Contact are the centerpiece of an intelligent and sustainable charging infrastructure for mode 3 electric vehicle charging.
Electronics housings with thermal simulation
Electronics housings with corresponding heatsinks and optimized PCB layouts offer optimal cooling and increased device performance. For BC, ME-IO, ICS, and UCS series electronics housings, Phoenix Contact therefore offers a combination of suitable heatsinks and a unique simulation service that maximizes the thermal efficiency of the device.
Caparoc circuit breaker system: New feed-in module with Modbus/TCP communication interface
The possible applications of the Caparoc circuit breaker system have been extended. With the new feed-in module with Modbus/TCP interface, the system can be used in other communication systems.
Convenient wiring of control cabinets with Push-X and Combi plug-in zone
The new pluggable terminal blocks with Push-X connection and Combi plug-in zone from Phoenix Contact set new standards in wiring technology. This combination enables effortless and efficient wiring in control cabinet building by connecting the field level with preassembled COMBI connectors.
IFS PROFIsafe Gateway for the easy network integration of up to 15 motor starters
The IFS PROFIsafe Gateway from Phoenix Contact makes it easy to integrate network-compatible motor starters into PROFIsafe networks and use them in safety applications.
Functional safety up to SIL 3 in potentially explosive areas
The configurable safety modules of the PSRmodular XC product family from Phoenix Contact have been certified for use in potentially explosive areas. This extends the range of applications further.
mGuard Secure Cloud version 3.1 is released
The mGuard Secure Cloud from Phoenix Contact allows secure remote access to machines and systems worldwide. Version 3.1 is now available with immediate effect.
New single-position VALVETRAB SPP surge protection
The type 2 surge protection devices from Phoenix Contact’s Safe Protection Plus (SPP) product family are now also available in single-position versions. This adds five ready-to-install products to the existing series, each of which is available with and without a remote indication contact.
The right choice with the new online configurator for system cabling for controllers
The new online configurator for system cabling for controllers from Phoenix Contact supports the quick and easy selection of a tailored system cabling solution.
Awards for the PLC-INTERFACE relay circuit breaker in the USA
The PLC-INTERFACE relay with circuit breaker from Phoenix Contact wins Gold at the Control Engineering 2025 Product of the Year Awards and the title “Most Valuable Product” at the Plant Engineering 2025 Product of the Year Awards in the USA.
Energy Management Service - On-Premises: Efficient energy management in accordance with ISO 50001 for sustainable corporate management
The energy management solution “Energy Management Service - On-Premises” is the focus of a strategic partnership between Phoenix Contact and EMPURON. The software provides powerful analysis tools that make it possible to evaluate energy data comprehensively and produce informative reports. This helps you make informed decisions about how to save energy.
Angled M12 device connector for THR
Phoenix Contact offers angled M12 connectors for reflow (THR) processing that have been specially developed for automated production.
Uno Power power supplies – new versions with Push-in and extended voltage range
Phoenix Contact is adding new power supplies to its portfolio: the Uno Power power supplies up to 90 W with Push-in connection technology and an extended voltage range up to 277 V AC. They are the optimum supply solution for 1-phase applications in compact control cabinets. The new power supplies from 30 to 90 W feature high power density, efficiency, and Push-in connection. This makes them ideal for industrial applications and compact control cabinets.
Phoenix Contact and TECSAFE: Better organization and efficiency with individual shadow boards for hand tools
Phoenix Contact’s collaboration with TECSAFE offers an additional opportunity to provide individual solutions that enable improved organization and greater efficiency.
New battery-pole connectors for residential storage systems
Phoenix Contact is introducing new connectors for residential storage applications to the market. Mechanical coding and color coding make the new connectors fit for use on battery inverters.
Multifunctional safety relay: Two protective functions in one device
With the PSRuni multifunctional safety relay from Phoenix Contact, up to two safety functions can be monitored with just one device. The comprehensive coverage of common safety functions allows flexible configuration and adaptation to individual requirements.
Device and Update Management on Docker Hub
With the Phoenix Contact Device and Update Management service based on OPC UA, it is possible to manage and update automation devices regardless of their manufacturer. The software, which was previously available as a Windows service, is now also available as a Docker container for use in Linux systems.
Environmental monitoring as the basis for demand-oriented irrigation
It has always been important to use water responsibly, and this is especially true in times of climate change. Comprehensive environmental monitoring is the first step towards making extreme events such as flooding or drought more manageable. In urban environments, for example, soil moisture is measured in green spaces. This is how demand-oriented irrigation is realized.
New IO-Link couplers for contactless power and data transmission
Phoenix Contact is adding new IO-Link couplers to its portfolio for contactless power and data transmission. The innovative product enables contactless data exchange between IO-Link devices in existing automation systems and offers numerous advantages for users.
New compact IO-Link device I/O boxes for field installation
The new IO-Link device I/O boxes from Phoenix Contact add robust devices to the portfolio for the Axioline E product family. They offer digital signal processing and flexible connection options for demanding environments.
Ready-to-install device combiner boxes for rooftop and ground-mounted PV systems
In the All Electric Society, green electricity is available reliably at all times and at affordable prices. Along with wind power, solar power makes a significant contribution to generating renewable energy. Experts who plan and install PV systems must ensure their high availability and performance. To this end, Phoenix Contact provides string combiner boxes (SCBs) from the Solarline product range for both small rooftop systems and for large ground-mounted systems.
360° security concept for the comprehensive protection of products, solutions, and services
When it comes to data acquisition in PV systems and wind turbine generators, the security of access to the collected data and the transmission paths is also extremely important. In addition to the ever-increasing risk of hacker attacks, there are various legal regulations aimed at protecting your company from cyberattacks. These include the Cyber Resilience Act, the NIS-2 Directive, and the KRITIS Regulation. Currently, there is not a harmonized standard for their implementation. However, it can be assumed that the internationally leading OT security standard IEC 62443 will play a decisive role.
CCS charging inlets with assembled cable set: the ready-to-install solution for electric vehicles
The CHARX connect universal CCS charging inlets for universal use from Phoenix Contact function as a High Power Charging interface with charging powers of up to 700 kW, significantly reducing charging times for electric vehicles and mobile machinery. The CCS type 2 charging inlets with assembled cable set are now available as a ready-to-install solution for electric vehicles for the first time.
CCS megawatt charging cables for up to 1,000 kW – High Power Charging reinvented
The second generation of the liquid-cooled CHARX connect professional HPC charging connectors from Phoenix Contact transmits up to 1 MW in boost mode. With this charging power, not only are electric vehicles charged in just a few minutes, but also utility vehicles with large batteries can be quickly ready for use again.
The smarter E Europe: Shaping the energy transition together with technical solutions
In order to achieve the climate targets, CO2 emissions must be reduced to a minimum in the next few years. Phoenix Contact is responding to this challenge with its vision of the All Electric Society. This vision describes a world in which electric energy from renewable resources is affordable and available in sufficient quantities at all times. To achieve this goal, the company offers technical solutions, products, and services.
Color RJ45 patch cables for CAT6A applications
Phoenix Contact is extending its product portfolio with color patch cables from the RJ45 Building series, which have been specially developed for applications in control cabinets. The new cables are available in eight colors: white, orange, yellow, red, violet, green, blue, and black.
PRC 20 series pluggable power distributor
The new pluggable power distributor from Phoenix Contact for up to 20 A is the ideal solution for quick and easy installation via plug-and-play.
Highly compact Mini Analog Pro Ex i signal conditioners and measuring transducers with comprehensive approval package
In addition to ATEX/IECEX and CCC Ex, the intrinsically safe 6.2 mm signal conditioners and measuring transducers from the Mini Analog Pro product family from Phoenix Contact now have further certifications.
Improved safety with line fault monitoring
On the basis of the new resistor network from Phoenix Contact, floating contacts and proximity switches can be used in combination with input modules in accordance with NAMUR IEC/EN 60947-5-6 for line fault monitoring. This proves to be indispensable in applications with high safety requirements.
Konfigurator zur individuellen Beschriftung von Kennzeichnungsmaterialien
Mit der Markierungslösung Marking Configurator von Phoenix Contact können individuell beschriftete Markierungsmaterialien für die Kennzeichnung von Klemmen, Leitern und Kabeln sowie Geräten und Anlagen bestellt werden. Der Konfigurator zeichnet sich durch seine hohe Benutzerfreundlichkeit und Flexibilität bei der individuellen Gestaltung von Kennzeichnungslösungen aus. Der Bestellprozess ist einfach, transparent und vollständig digitalisiert – und das bereits ab Stückzahl eins.
Multifunctional safety relays: two protective functions in one device
With the PSRuni multifunctional safety relay from Phoenix Contact, up to two safety functions can be monitored with just one device. The coverage of common safety functions enables flexible configuration and adaptation to individual requirements.
New resistance temperature measuring modules for Axioline F and Axioline P
Phoenix Contact is extending the portfolio of Axioline F and Axioline P remote I/O systems with three new resistance temperature measuring modules (RTD modules) that support resistive temperature measuring devices.
New lower housing part for ICS series electronics housings
With a width of 50 mm, the new lower housing part for the ICS series from Phoenix Contact provides the largest possible PCB surface and thus creates more space for the electronics it holds.
Versatile in use – the new universal tools
The Unifox tool portfolio from Phoenix Contact has been extended to include two new multifunctional pliers, three pliers wrenches, and one “Linemans” pliers.